- Studio 5000 View Designer Help
- Add a graphic element to a project
- Graphic elements library
- Reuse content
- Add-On Graphics
- Change a property
- Bind properties
- Display Automatic Diagnostics
- Use the runtime application
Unable to paste element type
Possible cause and solution:
- Copying an instance of an Add-On Graphic into the definition of an Add-On Graphic is not allowed.Paste a graphic element instead.
- Copying content from a predefined system management screen into the definition of an Add-On Graphic is not allowed.Paste system management screen content only in its original location to recover default project screens. Paste a different graphic element into the definition of the Add-On Graphic.
Provide Feedback