- Studio 5000 View Designer Help
- Add a graphic element to a project
- Graphic elements library
- Reuse content
- Add-On Graphics
- Change a property
- Bind properties
- Display Automatic Diagnostics
- Use the runtime application
Cannot perform operation on alarm table
Possible cause and solution:
- If the buttons on the alarm table appear available and without hash marks, the alarm table graphic element is read-only due to the assigned security role.Have the System Administrator grant the assigned security role access to the table.
Provide Feedback