- Studio 5000 View Designer Help
- Add a graphic element to a project
- Graphic elements library
- Reuse content
- Add-On Graphics
- Change a property
- Bind properties
- Display Automatic Diagnostics
- Use the runtime application
Performance is poor on HMI device
Possible cause and solution:
- The configuration of the project deployed to the HMI device may be too large.Tune the HMI device for optimized memory and limit the data the project displays.
Provide Feedback