- Studio 5000 View Designer Help
- Add a graphic element to a project
- Graphic elements library
- Reuse content
- Add-On Graphics
- Change a property
- Bind properties
- Display Automatic Diagnostics
- Use the runtime application
Popup does not open
Possible cause and solution:
- The popup no longer exists in the project.Recreate the popup inStudio 5000View Designer.
- The popup is renamed.Rename the popup, or on theEventstab for the selected screen or graphic element, select the popup that the event is to open.
- An event is not configured to open the popup.Verify on theEventstab of the selected graphic element that there is a Navigation event for opening the popup.
- Security access to the popup is not granted.Have the System Administrator grant your assigned security role access to the popup.
See also
Provide Feedback