Export Alarm history

Export Alarm history

Export the alarm history from the HMI device to removable media to view the alarm state changes collected on the HMI device. Open the exported alarm history file on a computer.
Prerequisites
  • Insert an SD Card or a USB drive into the HMI device so the Alarm Log service can export.
To export the alarm history
  1. Open the
    Settings
    screen.
  2. Select
    Data Export
    . The
    Data Export
    popup opens.
  3. In
    What to export,
    select
    Alarm history
    .
  4. In the
    Filename
    box, enter a name for the export file. "
    archive_alarms
    "
    is the default name of the export file.
  5. In
    Destination
    , select
    SD Card
    or
    USB Device
    .
  6. Select
    Export
    .
    Export progress
    shows a progress bar. The
    Data Export
    popup displays the last date and time a data log or alarm history exported at the top of the window.
    TIP:
    Tips:
    • When the alarm history is exporting, Data Log Exporting
      Data Export
      appears in the
      System Banner
      .
    • If there is an error in logging data or exporting, Data Log Error
      Data Export Error
      appears in the
      System Banner.
    • Data exports do not complete or create a .zip file on removable media if a ControlFLASH, reboot, or power cycle to the HMI device occurs during the export or when removing media before the export is complete.
    • There is no potential damage to files when removing a USB storage device when exporting data completes.
IMPORTANT:
Do not remove an SD card before preparing the media for safe removal. This may corrupt files on the removable device if the HMI device has data logging configured.
  1. If an SD card contains the exported alarm history file, next to
    SD Card
    , select Safely Remove icon
    Safely Remove SD Card
    . The
    Data Logger
    status at the top of the
    Data Export
    popup changes to
    Stopped
    and
    Remove SD card; reinsert to resume logging data
    appears.
    Data Log Exporting .
    Data Export Remove
    appears in the
    System Banner
    . It is safe to remove the SD card.
    TIP:
    Tips:
    • When exporting the alarm history to an SD card or USB storage device, avoid error messages by ensuring that the SD card or USB storage device:
      • has sufficient space
      • is inserted into the HMI device
      • has write permissions
      • is a supported SD card type
      • has a supported format of either FAT32 or EXT3
      • is not corrupted and does not contain corrupted files
    • If data does not export to a supported SD card that meets requirements, reboot the HMI device. If rebooting fails, insert the SD card into a computer and verify that the SD meets requirements. Follow any prompt to scan and repair the file system index on the SD card.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.