Open an alarm screen

Open an alarm screen

Open an alarm screen to view alarms and perform operations, such as acknowledging or shelving an alarm. Open the predefined
Alarm Summary
screen to view the Alarm Summary table. Open the predefined
Alarm Manager
screen to view the Alarm Manager table. Depending on the configuration of the HMI device application, alarm tables may exist on screens other than predefined screens.
To open an alarm screen
  • Alarm Summary.
    In the
    System Banner
    at the top of the screen, select
    Alarm Status Indicator
    Icon: ViewRTAlarmSumInAlUnackIcon. The
    Alarm Summary
    screen opens. The
    Alarm Status Indicator
    button turns red and flashes if there are unacknowledged alarms. The button stops flashing when there are no unacknowledged alarms.
  • Alarm Manager.
    In the
    System Banner
    at the top of the screen, select
    Navigation
    Icon: NavigationMenuButton and in the
    Navigation menu
    at the bottom of the screen, select the
    Alarm Manager
    item. The
    Alarm Manager
    screen opens.
    TIP:
    Tips:
    • To open the
      Alarm Manager
      screen from the
      Alarm Summary
      , select
      Alarm Manager
      viewrtalarmoptsmgrbuttonV5 at the bottom of the Alarm Summary table.
    • Using an external keyboard, tab to highlight a button on an alarm table and press
      Enter
      .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.