- Studio 5000 View Designer Help
- Add a graphic element to a project
- Graphic elements library
- Reuse content
- Add-On Graphics
- Change a property
- Bind properties
- Display Automatic Diagnostics
- Use the runtime application
Log data
If the
View Designer
project on the HMI device contains data logs, the HMI device logs the values of the tags in the data log automatically. The HMI device must have an SD card in order to log data. The SD Card allows the Data Log service to run and export. To log data
- Insert an SD Card into the HMI device.TIP:Tips:
- If a referenced tag does not exist in the controller or there is a communication issue with the controller,Tags are in errorappears at the top of theData Exportpopup of theSettingsscreen.
- Ejecting and immediately reinserting the SD card into the HMI device may not restart data logging. Data logging does not recognize that the SD card is present. Eject the SD card, wait several seconds, and reinsert the SD card to restart data logging.
Provide Feedback