- Studio 5000 View Designer Help
- Add a graphic element to a project
- Graphic elements library
- Reuse content
- Add-On Graphics
- Change a property
- Bind properties
- Display Automatic Diagnostics
- Use the runtime application
Error list contents
An
appears on the graphic element or group. This icon opens the
Error list
appears for any graphic element or group of graphic elements in error. An Error
icon 
Error list
. The item in error can be a graphic element, popup, or an Alarm Summary
or Alarm Manager
. 
Item | Description |
![]() | The number of graphic elements in error. An individual graphic element in error shows no number on the Error icon ![]() Error icon ![]() Error list contains a page of diagnostic messages for each graphic element in the group. |
![]() | The name of the graphic element affected by the current page of errors. Scroll horizontally to view long names. |
![]() | The diagnostic messages for the item in error.
|
![]() | When selected, the graphic element in error appears filled with a color that contrasts the background color of the screen. |
![]() | When there are multiple graphic elements in error, numbers indicate the graphic element. If there are three graphic elements in error while viewing diagnostic messages for the first graphic element, the Error list displays 1/3. The Next and Previous buttons show the diagnostic messages for the next and previous graphic elements. |
Provide Feedback