- Studio 5000 View Designer Help
- Add a graphic element to a project
- Graphic elements library
- Reuse content
- Add-On Graphics
- Change a property
- Bind properties
- Display Automatic Diagnostics
- Use the runtime application
HMI device keypad
Some
PanelView
5000 family of HMI devices have a physical keypad next to the screen. To use a physical keypad instead of the Virtual Standard Keypad
, use the physical keypad to enter numbers in an input element or dialog box. Use the physical keypad to interact with graphic elements. For example, use the physical keypad to select an item in a List Box Selector, select an alarm in an alarm table, open items in the Navigation menu
, and scroll messages in an Error list
. 
Item | Name | Description |
![]() | Function keys | Perform specific commands if events are configured for a screen or any of its graphic elements. For example, L1 could be configured in View Designer to navigate to another screen. |
![]() | Backspace | Press ![]() |
![]() | Enter | Press ![]() Input field at the top of the virtual keyboard or keypad. For example, if the cursor is in the Input field, pressing this button creates a blank line. Pressing this button while 1 is highlighted, enters 1 in the Input field. |
![]() | Tab | Press ![]() Input field on the virtual numeric keypad to the individual keys on the virtual numeric keypad. |
Back Tab | Press ![]() Navigation menu , press this key to move to an upper row in the Navigation menu . | |
![]() | Navigation | Press ![]() Navigation menu . |
![]() | Home | Press ![]() Input field, select the first item in a List Box Selector, or select the first alarm in an Alarm Summary or Alarm Manager table. |
End | Press ![]() Input field, select the last item in a List Box Selector, or select the last alarm in an Alarm Summary or Alarm Manager table. | |
![]() | Arrow keys | Press an arrow key to highlight the key directly above, below, or to the left or right of the currently highlighted key on the virtual standard keyboard. Press these keys to move one character at a time in the Input field of the virtual standard keyboard. |
![]() | Page Up | Press ![]() |
Page Down | Press ![]() | |
![]() | Esc | Press Esc to close a popup. |
Provide Feedback