Single-control solution from Rockwell Automation improves well pad functionality
MILWAUKEE — Drilling advancements, including horizontal drilling techniques, have transformed oil and gas operations from simplistic single-well pad fields to more complex multi-well pads. In turn, operators and equipment builders can modify their control systems approach to optimize these changing applications. The Well Manager solution from Rockwell Automation provides oil and gas companies a single solution for all control functionality throughout a
Traditionally, oil and gas companies built multi-well pads using different controls and locations throughout a single pad. The Rockwell Automation solution leverages just one controller for all
Click to download
“Today’s modern, multi-well pads resemble small production facilities,” said Marcus Toffolo, global sales lead for Oil and Gas, Rockwell Automation. “As such, traditional approaches for
The Well Manager solution is delivered pre-engineered to speed integration of a multi-well pad. It is scalable and can support up to 32 wells in one location with flow management, artificial lift control, and site-wide data visibility. Because data is pulled directly from the control system, it has higher integrity than operations that leverage manual data reporting. The solution is built with expansion in mind – ready to support wells and equipment that might be added to a site years after initial implementation.
The solution also enables self-declaring wells to be automatically discovered and integrated into the production environment. This auto-discovery feature removes human interaction, reducing
The Well Manager solution is part of the broader ConnectedProduction offering from Rockwell Automation that can help connect all existing automation systems and intelligent field equipment from the wellhead and surface processing to custody transfer. Users can select specific solutions as needed, and monitor ROI to justify scaling up for broader usage. Each added segment of the solution is purpose-built for connectivity to help transform data into useful intelligence. The offering makes use of current
The full ConnectedProduction offering including the Well Manager solution will be showcased and demonstrated using live customer examples at the upcoming Automation Fair event from Rockwell Automation on Nov. 15 and 16 in Houston.
About Rockwell Automation
Rockwell Automation Inc. (NYSE: ROK), the world’s largest company dedicated to industrial automation and information, makes its customers more productive and the world more sustainable. Headquartered in Milwaukee, Wis., Rockwell Automation employs approximately 22,000 people serving customers in more than 80 countries.
Media Contacts
John Heckman
Rockwell Automation
440.646.4096
jtheckma@ra.rockwell.com
Molly O’Mara
Padilla
612.455.1918
molly.omara@padillaco.com
Automation Fair and ConnectedProduction are trademarks of Rockwell Automation Inc.
Published November 9, 2017