Expanding on its partnership with Claroty, Threat Detection Services from Rockwell Automation featuring the Claroty xDome platform provide a highly flexible solution to help secure operational technology (OT) environments.
Completely scalable to meet needs as they evolve, this cloud-based platform allows remote or on-site deployment, enabling users to keep an eye on their most important data and assets, even from afar.
xDome Key Benefits:
- Extends cybersecurity across industrial xTended Internet of Things (XIoT)
- Supports the complete industrial cybersecurity journey
- Designed for scalability, flexibility, and ease-of-use
- Integrates seamlessly with existing technology stacks
OT expertise from Rockwell Automation coupled with Claroty xDome provides a customizable, full-service threat detection solution to help detect cyberattacks before they occur. Learn moreĀ here.
Published October 27, 2023