Configure a grid
Configure a grid or table to show or hide data. For example, show only the columns in the Tag Editor so the grid contains only the data you want to see. Do this to more quickly determine the tag values used in a manufacturing system.
To configure a grid
- Hide a column. Right-click a column heading and selectHide column. The column does not appear in the grid.
- Show a column. Right any column heading, selectToggle column, and then select the column to show. The column appears in the grid.
Provide Feedback