View tags and parameters for a device
From the
Device List
, open the tag editor to view tags and parameters for a controller or other device. - On the explorer bar, selectDevices.
- InDevicesexplorer, selectDevice list.
- Right-click a controller and selectView application tags and parameters, or right-click another device and selectView tags. The Tag Editor opens and lists the tags and parameters specific to that device.
Provide Feedback