Develop a script that exports table data to CSV

This script populates table columns with data and export that data to a
CSV
file.
Application example
NOTE:
Download a sample project:
ExampleApplication-ExportTableDataToCSV.zip
Prerequisites
In
FactoryTalk Optix Studio
, select
Run
to run the project using the client emulator to test your project. To run the project on a remote client, see Add a client device.
TIP: When you generate and export data, the CSV file is saved to the following folder:
%localappdata%\Rockwell Automation\FactoryTalk OptixEmulator\Projects\ExportTableDataToCSV\ApplicationFiles\
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.