- Getting started
- Using the software
- OPC UA
- Graphic and layout objects
- Developing solutions
- Developing projects with C#
- Application examples
- UI tutorial
- NetLogic tutorial
- Object and variable references
Create a variable
Create a variable that indicates the current temperature.
- Create the variable:
- InProject view, right-clickModeland select .
- Hover-over the variable, select, and enterTemperature.
- Configure the variable:
- InProperties, selectInt32and selectFloat.
- Right-clickTemperatureand select .
- UnderEURange, setHigh limitto100.
Provide Feedback