Develop buttons for closing the application and shutting down the host system

Create a check box that shows or hides a clock label, which state is persistent based on the currently logged in user.
IMPORTANT:
Pressing the
Shut down system
button
immediately shuts down the host operating system
on which the
FactoryTalk Optix Application
runs.
For example, if you run the
FactoryTalk Optix Application
on an emulator target, pressing the button will immediately shut down your Windows system.
Application example
Prerequisites
Application design example
In
FactoryTalk Optix Studio
, select
Run
to run the project using the client emulator to test your project. To run the project on a remote client, see Add a client device.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.