Develop buttons for closing the application and shutting down the host system
Create a check box that shows or hides a clock label, which state is persistent based on the currently logged in user.
IMPORTANT:
Pressing
Shut down system
immediately shuts down the host operating system
on which the FactoryTalk Optix Application
runs.For example, if you run the
FactoryTalk Optix Application
on an emulator target, pressing Shut down system
immediately shuts down your Windows system.
TIP:
Download a sample project:
ExampleApplication-CloseApplicationShutDownSystem.zipPrerequisites
- To develop the project
- Arrange the interface elements.
- Save the project.
In
FactoryTalk Optix Studio
, select to run the project using the client emulator to test your project. To run the project on a remote client, see Add a client device.Provide Feedback