Test the OPC UA server with a UaExpert client
The UaExpert® application is distributed by Unified Automation®. You can download the application after registration.
Prerequisites
Do the following:
- Download and install UaExpert from https://www.unified-automation.com/downloads/opc-ua-clients.html.For more information on how to install and use UaExpert, see the Unified Automation documentation.
- InFactoryTalk Optix Studio, add and configure the OPC UA server object. See Add an OPC UA server object.
- Run a project in theEmulatorclient. See Add a client device.
Provide Feedback