Create a list box
Create a list box that enables you to switch between Motor and Kiln objects.
- InProject view, right-clickMainWindow (type)and select .
- InProperties, create a dynamic link betweenModeland .For more information about dynamic links, see Create dynamic links.
- ExpandModeland create a dynamic link betweenItemKindand .For more information about dynamic links, see Create dynamic links.
Provide Feedback