Deploy a FactoryTalk Optix Application from a folder

Deploy a FactoryTalk Optix Application from a folder

To deploy a
FactoryTalk Optix Application
from a folder on a shared drive or a USB drive, move the file to the client device and run the file.
  1. Move the file from the shared drive to the client device.
  2. Run
    FactoryTalk Optix Application
    on the client system:
    • On
      Windows®
      client devices, double-click
      FTOptixRuntime.exe
      .
    • On Linux client devices, in the terminal, navigate to the
      FTOptixRuntime
      file folder and enter
      ./FTOptixRuntime
      .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.