- Getting started
- Using the software
- OPC UA
- Graphic and layout objects
- Developing solutions
- Developing projects with C#
- Application examples
- UI tutorial
- OPC UA tutorial
- NetLogic tutorial
- Object and variable references
Create a Presentation Engine
Add a Native Presentation Engine or a Web Presentation Engine to your project.
TIP:
Each
FactoryTalk Optix Studio
project can contain a single Native Presentation Engine and a single Web Presentation Engine.- InProject view, right-click a window object.
- Select one of the following options:
- To create a default Presentation Engine, select.
- To create a Web Presentation Engine, select.
- InProperties, set any required Presentation Engine properties.For more information, see Native presentation engine and Web presentation engine.
Provide Feedback