Configure the main panel (type)
Add and configure a panel loader that defaults to the speed panel.
- InProject view, right-clickMainPanel (type)and select
- Hover-over the panel loader, select, and enterMainPanelLoader.
- InPropertiespane, create a dynamic link betweenPaneland .For more information about dynamic links, see Create dynamic links.
Provide Feedback