Optix templates

Optix templates

Optix templates provide user-defined default content for projects to contain the same content as a starting point. You can then create a new project based on the template. Edit an Optix template by opening the template and modifying the content as desired. Optix templates have an .optixt extension and are prepended with FTOptix_template_ .
When you create or edit an Optix template, you can select
Run
to emulate the template like any other project. You can only deploy a project based on an Optix template to a runtime device.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal