Develop a UI that generates a PDF report
Generate a PDF report with a custom header and footer that contains information from a data grid.
Application example
![](/content/dam/dita/en/factorytalk-optix/current/_images/PDFReport.png/_jcr_content/renditions/original)
NOTE:
Download a sample project:
PDFReportWithDataGrid.zipPrerequisites
- To develop the project
- Arrange the interface elements.
- Save the project.
Application design
![](/content/dam/dita/en/factorytalk-optix/current/_images/PDFReportDesign2.png/_jcr_content/renditions/original)
Report design
![](/content/dam/dita/en/factorytalk-optix/current/_images/PDFReportDesign.png/_jcr_content/renditions/original)
Select
to run the project using the client emulator to test your project. To run the project on a remote client, see Add a client device.
Run
Provide Feedback