Backlash page
The settings on the
Backlash
page configure backlash options for the load of the motor. Use the settings to:- Enter theReversal Offsetvalue to compensate for positional inaccuracy introduced by mechanical backlash.
- Enter theCompensation Windowvalue to define a window around the command position.
TIP:
To open the Backlash page:
- In theController Organizer, expand theMotion Groupsfolder, and double-click an axis.
- From theAxis Propertiesdialog box, inCategories, expand theLoadfolder, and then clickBacklash.
Parameter | Description |
---|---|
Reversal Offset | Specifies the reversal offset for the load in terms of user-defined position units. |
Compensation Window | Specifies the compensation window in terms of user position units. |
Provide Feedback