Cyclic Parameters page

Use the
Cyclic Parameters
page to select the parameters to read and write at each update period. Monitor the parameters from the
Cyclic Parameters
page.
TIP: To open the Cyclic Parameters page:
  1. In the
    Controller Organizer
    , expand the
    Motion Groups
    folder, and double-click an axis.
  2. From the
    Axis Properties
    dialog box, in
    Categories
    , click
    Cyclic Parameters
    .
The
Cyclic Parameters
page includes these parameters.
Parameter
Description
Parameters to be read each cycle
Items to include in the cyclic read parameter list. Select the box to the left of the parameter to enable the parameter. Limited to 10 enabled selections.
Tip:
The associated
Value
field is blank in Offline mode. When in Online mode, the list shows only the enabled data with the correct value.
Parameters to be written each cycle
Items to include in the cyclic write parameter list. The
Parameters to be read each cycle
parameter determines what is in this list.
Select the box to the left of the parameter to enable the parameter. Limited to 10 enabled selections.
Tip:
The associated
Value
field is blank in Offline mode. When in Online mode, the list shows only the enabled data with the correct value.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.