Polarity page
Use the settings on the
Polarity
page in the Axis Properties
dialog box to choose polarity options for the actual motor.
TIP:
To open the Polarity page:
- In theController Organizer, expand theMotion Groupsfolder, then right-click the axis and selectProperties.
- From theAxis Propertiesdialog box, inCategories, selectPolarity.
Parameter | Description |
---|---|
Motion Polarity | Select Normal or Inverted for the polarity of the motion planner. |
Motor Polarity | Select Normal or Inverted for the motor polarity. Motor Polarity appears dimmed when the axis configuration is set to no feedback. It is enabled for all other axis configurations. |
Feedback 1 Polarity | Select Normal or Inverted for the polarity of the motor feedback device. Feedback 1 Polarity appears dimmed when the configuration is set to no feedback. |
Feedback 2 Polarity | Select Normal or Inverted for the polarity of the motor feedback device. Feedback 2 Polarity appears dimmed when the configuration is set to no feedback. |
Test Polarity | Opens the Motor & Feedback tab in the Hookup Tests dialog box.Test Polarity is unavailable in offline mode and online in Servo On mode. |
Provide Feedback