- Studio 5000 Logix Designer
- Tasks, programs, and routines
- Add-On Instructions
- Controller Organizer
- Logical Organizer
- Alarms
- Tag-based alarms
- Tag Editor and Data Monitor
- Configure settings for Tag Editor and Data Monitor
- Equipment phases
- Equipment Sequences
- Equipment Sequence Diagrams
- Ladder Editor
- Structured Text Editor
- Sequential Function Chart Editor
- Define the steps of an SFC process
- PlantPAx instruction properties
- Controller Properties
- Editing Controller Properties
- Controller Security
- Source Protection
- License Source Protection for Routines and Add-On Instructions
- Module Information
- 1756 ControlLogix I/O Modules
- Instruction Set
Status page
The
Status
page displays the current status of the axis and digital I/O.
TIP:
The available parameters depend on the
Axis Configuration
on the General
page and are blank when the device is offline.
TIP:
To open the Status page:
- In theController Organizer, expand theMotion Groupsfolder, and double-click an axis.
- From theAxis Propertiesdialog box, inCategories, clickStatus.
Parameter | Description |
Actual Position | The current axis position in the configured Position Units of that axis. This value is based on time stamped position or velocity feedback data reported to the controller as part of an ongoing cyclic data transfer process. |
Actual Velocity | The current speed and direction of an axis, in the configured axis Position Units per second. The actual velocity is calculated from the current increment to the actual position per Coarse Update Period. |
Command Position | The desired or commanded position of a physical axis, in the configured Position Units of that axis, as generated by the Motion Planner. |
Command Velocity | The commanded speed and direction of an axis, in the configured Position Units per second, as generated by the Motion. The command velocity is calculated as the current increment to the command position per coarse update interval. |
Axis Status | The LED next to each of the Axis States lights up when it reaches that state. For example, if the Torque Limit is reached, the light next to Torque Limit turns blue. If the limit is not reached, the light remains gray.Axis Statuses include:
|
Digital I/O | The LED next to each of the Digital I/O States lights up if it reaches that state. For example, if Registration 1 is reached, the light next to Registration 1 turns blue. If the limit is not reached, the light remains gray.Digital I/O States include:
|
Provide Feedback