Delete an Add-On Instruction from the Controller Organizer
Use the
Delete
command to remove an Add-On Instruction from the Controller Organizer
. These restrictions apply when deleting an Add-On Instruction:
- The Add-On Instruction must not be referenced.
- You must be offline because you cannot delete an Add-On Instruction when online.If you select multiple Add-On Instructions to delete, and any selected Add-On Instruction violates any of the restrictions, none of the selected Add-On Instructions are deleted.TIP: If FactoryTalk Security is enabled, FactoryTalk Security permissions are required to create and delete items in theController Organizerand theLogical Organizer.
To delete an Add-On Instruction from the
Controller Organizer
:- Right-click the Add-On Instruction, and then chooseDelete.
- ChooseYesto confirm the deletion.TIP:You can also delete an Add-On Instruction by selecting it and then using one of these methods:
- From theMenubar, selectEdit>Delete.
- Press theDeletekey.
For additional information about the
Controller Organizer
and the Logical Organizer
, see:Provide Feedback