- Studio 5000 Logix Designer
- Tasks, programs, and routines
- Add-On Instructions
- Controller Organizer
- Logical Organizer
- Alarms
- Tag-based alarms
- Tag Editor and Data Monitor
- Configure settings for Tag Editor and Data Monitor
- Equipment phases
- Equipment Sequences
- Equipment Sequence Diagrams
- Ladder Editor
- Structured Text Editor
- Sequential Function Chart Editor
- Define the steps of an SFC process
- PlantPAx instruction properties
- Controller Properties
- Editing Controller Properties
- Controller Security
- Source Protection
- License Source Protection for Routines and Add-On Instructions
- Module Information
- 1756 ControlLogix I/O Modules
- Instruction Set
Delete programs from the organizers
Use the
Delete
command to remove programs from the Controller Organizer
and the Logical Organizer
. Deleting a program from either organizer also deletes it from the other organizer. Deleting a parent program also deletes its descendant items.The
Controller Organizer
does not show the logical hierarchy, so the descendants of a program or phase appear at the same level under a task. The Logical Organizer
displays the logical model and shows the descendants of a program. A warning message appears when you try to delete a program with descendants in the Controller Organizer
because that organizer does not show the descendant relationships.These restrictions apply when deleting a program:
- When online, the controller must not be locked or in Hard Run mode.
- The program and all of its descendants must not have safety restrictions.
- The program must not have redundancy restrictions or security restrictions.TIP: if FactoryTalk Security is enabled, FactoryTalk Security permissions are required to create and delete items in theController Organizerand theLogical Organizer.
To delete a program or phase:
- If online, you must unschedule the program first.
- Right-click the program, and then chooseDelete.
- ChooseYesto confirm the deletion.TIP:You can also delete a program by selecting it and then using one of these methods:
- From theMenubar, selectEdit>Delete.
Press theDeletekey.
For additional information about the organizers, see:
Provide Feedback