Controller Properties dialog box - Security tab

Use the settings on the
Security
tab to configure these properties:
  • Security
  • Trusted slots
  • Enable or disable controller embedded web page
  • Component state tracking
  • Change detection
The settings on the
Security
tab are unavailable when:
  • The user does not have security permissions to edit the controller settings.
  • The controller is operating in Hard Run mode.
TIP: To open the Controller Properties dialog box - Security tab:
  1. On the
    Online
    toolbar, click the
    Controller Properties
    icon.
  2. On the
    Controller Properties
    dialog box, click the
    Security
    tab.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.