Transition expression verification
If the expression fails to verify, the
Unverified Indicator
is shown next to the transition name. There are two reasons a transition expression will not verify.Expression contains a term that is not a tag
For example, if you have configured
Tag1
through Tag10
, the expression Tag11>3
fails to verify because the value Tag11
is not configured and cannot be interpreted as a number.Expression evaluates to a non-Boolean value
For example, if you have an expression of the Boolean type, the value
1
verifies because it is evaluated as TRUE
. The expression Hello World
does not verify because it does not evaluate to a Boolean value. Tag1
verifies if Tag1
is a configured tag of type Boolean, but Tag2+1
does not verify because its result cannot be interpreted as a Boolean value.Provide Feedback