Series topology

A series topology consists of a linear ordering of steps and transitions. Steps in the sequence execute directly one after another in series without any branching or looping. The following example shows an Equipment Sequence diagram that uses a series topology.
Item
Name
Description
Initial step
When the sequence is commanded to START, this step becomes active.
Transition
When this transition becomes TRUE, the first step in the sequence becomes active.
Steps in series sequence
Each step becomes active and executes when its preceding transition becomes TRUE.
Transition
The last transition in the series.
End step
When the end step changes to COMPLETE, the Equipment Sequence becomes complete.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.