- Studio 5000 Logix Designer
- Tasks, programs, and routines
- Add-On Instructions
- Controller Organizer
- Logical Organizer
- Alarms
- Tag-based alarms
- Tag Editor and Data Monitor
- Configure settings for Tag Editor and Data Monitor
- Equipment phases
- Equipment Sequences
- Equipment Sequence Diagrams
- Ladder Editor
- Structured Text Editor
- Sequential Function Chart Editor
- Define the steps of an SFC process
- PlantPAx instruction properties
- Controller Properties
- Editing Controller Properties
- Controller Security
- Source Protection
- License Source Protection for Routines and Add-On Instructions
- Module Information
- 1756 ControlLogix I/O Modules
- Instruction Set
Equipment Sequence Properties - General tab settings
Use the
General
tab of the Equipment Sequence Properties
dialog box to modify the name, description, containing task, revision, revision note, and security setting of the Equipment Sequence. The following options are available on the General
tab.Parameter | Description |
Name | The sequence name, which must follow the IEC-61131 Name Standard. The application ignores
invalid characters. |
Description | Enter the optional description for this Equipment Sequence . Language switching is provided for this
control. |
Parent | Use the list to choose under which logical parent the Equipment Sequence is created. |
Schedule in | Displays the task that runs the Equipment Sequence program. |
Revision |
|
Revision Note | This is an optional field that allows text entry to further describe this Equipment Sequence
revision. For example, list the changes made to the Equipment Sequence since the last revision. |
Permission Set | Applies a set of permissions that controls access based on the permissions configured in FactoryTalk Security . The default setting, <Controller Inherited> , applies the same security settings that have been applied to the controller or project. |
Provide Feedback