Error - Failed to complete the check out operation

An error occurred in the check out process and the file was not checked out.
Possible causes include disk or user permission issues, network problems, and server authentication issues.
OK
Click this button to return to the Open/Import Project dialog.
Help
Click this button for help on this error.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.