Connection Properties dialog box - General tab
Use the
Connection Properties
dialog box to view the parameter and connection properties to determine if the connection is valid.Attributes
Parameter
Displays the properties of the endpoint of the connection. This is the parameter in the import content that is to be connected to another parameter in the program that exists in the project.
Connection
Displays the properties of the connection endpoint as read from the import file or project.
Current Operation
Displays the current operation selected for the connection, as displayed in the Connections grid.
Connect
Select this button to set the operation for the connection to
Connect
and close the dialog box.Disconnect
Select this button to set the operation for the connection to
Disconnect
and close the dialog box.Provide Feedback