Failed to set the maximum number of rows to display the rung comment. The valid range is 1 to 1000.

This message appears when pressing Apply or OK and the maximum number of lines entered to display for the rung comment is invalid or not within the valid range.
Enter a value between 1 and 1000.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.