PLLS active command source

Use the
Command Source
tab on the
PLLS Properties
dialog box to:
  • Select Program, Operator, Operator Locked, External, or Maintenance as the source of commands and settings for the instruction.
  • Set In Service or Out of Service as the command source state. The instruction only accepts device commands and settings from the selected source when the state is In Service.
To select the active command source for PLLS instructions
  1. On the instruction in the routine, perform one of these actions:
    • On the Ladder or FBD instruction, select .
    • In the Structured Text editor, right-click the tag name and select
      Configure <tag name>
      .
  2. Select the
    Command source
    tab.
    The
    Status
    indicator at the top of the tab:
    • Lists all potential command sources from highest priority on the left to lowest priority on the right.
    • Highlights all requesting command sources in black text.
    • Outlines the current command source for the instruction.
    • When the current command source releases its request, the next active requestor becomes the current command source.
  3. Set and clear command source requests:
    • Online command source request.
      When online, select the command source for the instruction. These commands take effect immediately.
      • Program
        . Select Program as the source of commands and settings for the instruction.
      • Operator.
        Select Operator as the source of commands and settings for the instruction.
      • Operator lock
        . Lock Operator as the command source. When Operator is locked, Program requests from logic are not accepted.
        IMPORTANT:
        Selecting Program when the command source is Operator Locked unlocks Operator and sets the Program command source request.
      • External/Release External.
        Select or release External as the source of commands and settings for the instruction.
      • Maintenance/Release maintenance
        . Select or release Maintenance as the source of commands and settings for the instruction.
    • In service/Out of service
      . Set In Service or Out of Service as the instruction command source state.
  4. View the read-only parameters:
    • Device state
      . When the
      Logix Designer
      application is online with the controller, the indicator displays the current device state:
      • None
      • Stopped
      • Running
      • Stopping
      • Decreasing
      • Increasing
    • Device issues
      . When the
      Logix Designer
      application is online with the controller, the indicator displays fault conditions:
      • None
      • Configuration error
      • Fail to start
      • Fail to stop
  5. Select
    Apply
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.