- Studio 5000 Logix Designer
- Tasks, programs, and routines
- Add-On Instructions
- Controller Organizer
- Logical Organizer
- Alarms
- Tag-based alarms
- Tag Editor and Data Monitor
- Configure settings for Tag Editor and Data Monitor
- Equipment phases
- Equipment Sequences
- Equipment Sequence Diagrams
- Ladder Editor
- Structured Text Editor
- Sequential Function Chart Editor
- Define the steps of an SFC process
- PlantPAx instruction properties
- Controller Properties
- Editing Controller Properties
- Controller Security
- Source Protection
- License Source Protection for Routines and Add-On Instructions
- Module Information
- 1756 ControlLogix I/O Modules
- Instruction Set
Change Module Properties preferences
Use the
Print Options
dialog box to select the module properties information you want to include in your report.To change Module Properties preferences:
- From the main menu, selectFile>Print Options.
- From thePrintdialog box, selectPrint Options.
- Select theModule Properties Listingcategory and select or clear the following:
- Communications Path.Print module properties data grouped by backplane and network membership.
- Controller Organizer Tree.Print module properties data in the order depicted in the Controller Organizer.
- SelectOK.
Provide Feedback