Generate Report dialog box settings
Use the
Generate Report
dialog box to create and print reports for components in the Controller Organizer. You can create a report for one component or for several components at once.The following table describes the parameters available:
Parameter | Description |
Component Selection | Displays the components in your project for which you can generate a report. When a component is selected, a selection icon appears in the component check box. |
Report Selection | Displays the reports you can generate for the selected components. |
Print Options | Opens the Print Options dialog box. |
Page Setup | Opens the Page Setup dialog box. |
Print | Confirms your selections, prints the reports, and closes the Generate Report dialog. |
Component Selection details
Icons used in the Component Selection area:


not
selected, but some (not all) of its children are selected.

You can select the following components. When you select a child of a folder, the folder is automatically selected.
- Project- The controller, tags, routines, add-on instructions, and I/O Configuration are all children of this component.
- Controller- The controller for the project.
- Tags- Controller and program-scoped tag collections of your project are children of this selection. Only tag collections that have tags defined are listed under this selection.
- Routines- Tasks are children of this category. Each program in the task is a child of the task, and each routine in a program is a child of the program.
- Add-On Instructions- The Add-On Instruction category is not displayed unless you include at least one Add-On Instruction in your project.
- Data Types- User-defined data types, strings, predefined data types, and module-defined data types are children of this component.
- I/O Configuration- The backplane and each of its components are all children of this component.
Report Selection details
The reports you can generate include the following.
- Table of Contents- Include a table of contents in your report. By default, the table of contents appears at the end of a report.
- Controller- There are two controller reports — Controller Organizer Listing and Controller Properties Listing. These reports only appear if you select theProjectcomponent.
- Tag- There is one tag report — Tag Listing. This report appears only if you select theTagscomponent.
- Tasks- There is one task report — Tasks Properties Listing. This report appears only if you select theRoutinescomponent.
- Program/Phase- There is one program/phase report — Program/Phase Properties Listing. This report appears only if you select theRoutinescomponent.
- Routine- The routine reports include Routine Listing, Tag Listing for Routine, Sequencing and Step Tag Listing, and Routine Properties Listing. These reports only appear if you select theRoutinescomponent.
- Add-On Instructions- There are two potential add-on instruction reports — Add-On Instruction Definition and Add-On Instruction Signature Listing. The Add-On Instruction Signature Listing report appears only if you select theAdd-On Instructionscomponent. The Add-On Instruction Definition report appears only if you select a child of theAdd-On Instructionsfolder.
- Data Type- There is one data type report — Data Type Listing. This report appears only if you select theData Typescomponent.
- Module Properties- There is one module properties report — Module Properties Listing. This report appears only if you select theI/O Configurationcomponent.
- OPC UA- The OPC UA report indicates whether the controller supports OPC UA and if so, for which controller ports.
Provide Feedback