Safety Lock/Unlock dialog box

Safety Lock/Unlock dialog box

Use the
Safety Lock/Unlock
dialog box to change the lock state of the Safety application. Locking the Safety application protects the application from unauthorized changes, and prevents editing of safety components, such as safety task, safety programs, safety routines, safety Add-On Instructions, safety tags, safety I/O, and safety task signature.
TIP:
Do one of the following to open the Safety Lock/Unlock dialog:
  • Select
    Tools
    >
    Safety
    >
    Safety Lock/Unlock
    .
  • On the
    Online
    toolbar, select the
    Controller Properties
    icon. On the
    Controller Properties
    dialog box, select the
    Safety
    tab, and then select
    Safety Lock/Unlock
    .
The
Safety Lock/Unlock
dialog box and the parameters will vary, depending on the current state of the application (that is, if the application is currently locked, the dialog box will appear as the
Unlock
dialog box, and vice versa).
Parameter
Description
Enter Password
Password, if one exists, for the state to which you want to change. There is a separate password for the Lock and Unlock state.
Password is no longer than 40 characters, and is not case sensitive. It may include letters A-Z (upper and lower case), numerals 0-9, and the following symbols:
` ~ ! @ # $ % ^ & * ( ) _ + , - = { } | [ ] \ : ; ? /.
Generate Safety Signature
Determines whether a new Safety signature is generated when the Safety application is locked.
Only available when the controller is online.
Lock
Locks the Safety application to protect it from modifications and creates a Safety signature if the
Generate Safety Signature
check box
is selected.
Delete Safety Signature
Determines whether the current Safety signature information is deleted when the Safety application is unlocked.
Unlock
Unlocks the Safety application to allow editing and forcing in the Safety application and deletes the Safety signature if
Delete Safety Signature
check box is selected.
Change Password
Opens the
Change Passwords
dialog box to create a password or modify the existing password for the Lock and Unlock states.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal