- Studio 5000 Logix Designer
- Tasks, programs, and routines
- Add-On Instructions
- Controller Organizer
- Logical Organizer
- Alarms
- Tag-based alarms
- Tag Editor and Data Monitor
- Configure settings for Tag Editor and Data Monitor
- Equipment phases
- Equipment Sequences
- Equipment Sequence Diagrams
- Ladder Editor
- Structured Text Editor
- Sequential Function Chart Editor
- Define the steps of an SFC process
- PlantPAx instruction properties
- Controller Properties
- Editing Controller Properties
- Controller Security
- Source Protection
- License Source Protection for Routines and Add-On Instructions
- Module Information
- 1756 ControlLogix I/O Modules
- Instruction Set
Add a step to an SFC
Add a step to a Sequential Function Chart to change its process logic.
To add a step to an SFC:
- SelectStep + Transfer
.
- If theLogix Designerapplication is configured to prompt for the names of SFC tags, then type a name for the step.
- Choose the scope for the tag of the step.
- SelectOK.
- Type a name for the associated transition.
- Choose the scope for the tag of the step.
- SelectOK.A step and transition pair is created.
Provide Feedback