Create a motor values widget instance

Create a motor values widget instance from the motor values widget type.
  1. In the
    Project view
    pane, right-click
    MainWindow (type)
    and select
    New
    MotorValuesWidget
    .
  2. In the
    Properties
    pane, create a dynamic link between the
    Motor
    property and
    ProjectName
    UI
    MainWindow (type)
    MotorListBox
    Selected item (Pointer)
    .
    For more information about dynamic links, see Create dynamic links.
Fornire un feedback
Hai domande o feedback su questa documentazione? invia il tuo feedback qui.