Create a speed gauge and labels
Create UI elements that display speed-related information about a selected motor.
- Create the speed gauge:
- In theProject viewpane, right-clickMotorSpeedPaneland select .
- Hover-over the gauge, select, and enterSpeedGauge.
- In thePropertiespane, create a dynamic link between theValueproperty and .For more information about dynamic links, see Create dynamic links.
- Create the speed label:
- In theProject viewpane, right-clickMotorSpeedPaneland select .
- Hover-over the label, select, and enterSpeedLabel.
- In thePropertiespane, set theTextproperty value toSpeed.
- Create the speed value label:
- In theProject viewpane, right-clickMotorSpeedPaneland select .
- Hover-over the label, select, and enterSpeedValueLabel.
- In thePropertiespane, create a dynamic link between theTextproperty and .For more information about dynamic links, see Create dynamic links.
Fornire un feedback