Create an acceleration gauge and labels
- Create the speed gauge:
- In theProject viewpane, right-clickMotorAccelerationPaneland select .
- Hover-over the gauge, select, and enterAccelerationGauge.
- In thePropertiespane, create a dynamic link between theValueproperty and .For more information about dynamic links, see Create dynamic links.
- Create the speed label:
- In theProject viewpane, right-clickMotorAccelerationPaneland select .
- Hover-over the label, select, and enterAccelerationLabel.
- In thePropertiespane, set theTextproperty value toAcceleration.
- Create the speed value label:
- In theProject viewpane, right-clickMotorAccelerationPaneland select .
- Hover-over the label, select, and enterAccelerationValueLabel.
- In thePropertiespane, create a dynamic link between theTextproperty and .For more information about dynamic links, see Create dynamic links.
Fornire un feedback