Create a button that closes the application
Create a button that closes the
FactoryTalk Optix Application
application.- In theProject viewpane, right-clickMainWindow (type)and select .
- Hover-over the button, select, and enterCloseApplicationButton.
- In thePropertiespane, set theTextproperty value toClose application.
- In theEventspane, next toMouseClick event, selectand select .
Fornire un feedback