Create an analog variable
Create an analog variable that indicates temperature.
- In theProject viewpane, right-clickModeland select
- Configure the variable:
- In thePropertiespane, set theAnalogVariable1 (Float)property value to50.
- Next to the property value, select<None>and selectTemperature: degree Fahrenheit
- UnderEURange, set theLow limitproperty value to-10.
- Set theHigh limitproperty value to60.
- Set theConstrainproperty value toTrue.
Fornire un feedback