Create panels
Create a navigation panel that enables you to switch between two other panels.
- Create a SavePanel (type):
- In theProject viewpane, right-click theUIfolder and select .
- Hover-over the panel, select, and enterSavePanel.
- Create a ValuePanel (type):
- In theProject viewpane, right-click theUIfolder and select .
- Hover-over the panel, select, and enterValuePanel.
- Create a NavigationPanel:A navigation panel enables you to switch between different panels.
- In theProject viewpane, right-clickMainWindow (type)and select .
- In thePropertiespane, underPanel1, create a dynamic link between thePanelproperty and .For more information about dynamic links, see Create dynamic links.
- In thePropertiespane, next toPanels, select.
- In thePropertiespane, underPanel2, create a dynamic link between thePanelproperty and .For more information about dynamic links, see Create dynamic links.
Fornire un feedback