Create elements for controlling the current value

Create elements for controlling the current value

Create a gauge and other interface elements that display the current value and enable you to edit it.
  1. Create the current value label:
    1. In the
      Project view
      pane, right-click
      MainWIndow (Type)
      and select
      New
      Base controls
      Label
      .
    2. Hover-over a gauge, select
      Edit
      , and enter
      CurrentValueLabel
      .
    3. In the
      Properties
      pane and set the
      Text
      property value to
      Current Value
      .
  2. Create the value gauge:
    1. Right-click
      MainWindow (Type)
      and select
      New
      Base controls
      Linear gauge
      .
    2. Hover-over a gauge, select
      Edit
      , and enter
      ValueGauge
      .
    3. In the
      Properties
      pane, create a dynamic link between the
      Value
      and
      ProjectName
      Model
      ConstrainedVariable
      .
      For more information about dynamic links, see Create dynamic links.
  3. Set the value gauge warning zone 1:
    1. In the
      Properties
      pane, next to
      Warning zones
      , select
      Add
      .
    2. Under
      WarningZone1
      , set the
      Color
      property value to
      #f30000
      .
    3. Create a dynamic link between the
      From
      property and
      ProjectName
      UI
      MainWindow (Type)
      ValueGauge
      Minimum value
      .
      For more information about dynamic links, see Create dynamic links.
    4. Create a dynamic link between the
      To
      property and
      ProjectName
      Model
      ConstrainedVariable
      EURange
      Low limit
      .
      For more information about dynamic links, see Create dynamic links.
  4. Set the value gauge warning zone 2:
    1. Next to
      Warning zones
      , select
      Add
      .
    2. Under
      WarningZone2
      , set the
      Color
      property value to
      #02d92d
      .
    3. Create a dynamic link between the
      From
      property and
      ProjectName
      Model
      ConstrainedVariable
      EURange
      Low limit
      .
      For more information about dynamic links, see Create dynamic links.
    4. Create a dynamic link between the
      To
      property and
      ProjectName
      Model
      ConstrainedVariable
      EURange
      High limit
      .
      For more information about dynamic links, see Create dynamic links.
  5. Set the value gauge warning zone 3:
    1. Next to
      Warning zones
      , select
      Add
      .
    2. Under
      WarningZone3
      , set the
      Color
      property value to
      #f30000
      .
    3. Create a dynamic link between the
      From
      property and
      ProjectName
      Model
      ConstrainedVariable
      EURange
      High limit
      .
      For more information about dynamic links, see Create dynamic links.
    4. Create a dynamic link between the
      to
      property and
      ProjectName
      UI
      MainWindow (Type)
      ValueGauge
      Maximum value
      .
      For more information about dynamic links, see Create dynamic links.
  6. Create the value label:
    1. In the
      Project view
      pane, right-click
      MainWIndow (Type)
      and select
      New
      Base controls
      Label
      .
    2. Hover-over a gauge, select
      Edit
      , and enter:
      ValueLabel
      .
    3. In the
      Properties
      pane, create a dynamic link between the
      Text
      property and
      ProjectName
      Model
      ConstrainedVariable
      For more information about dynamic links, see Create dynamic links.
  7. Create the value spin box:
    1. In the
      Project view
      pane, right-click
      MainWIndow (Type)
      and select
      New
      Base controls
      Spin box
      .
    2. Hover-over a gauge, select
      Edit
      , and enter:
      ValueSpinBox
      .
    3. In the
      Properties
      pane, create a dynamic link between the
      Value
      property and
      ProjectName
      Model
      ConstrainedVariable
      For more information about dynamic links, see Create dynamic links.
  8. Create the value text box:
    1. In the
      Project view
      pane, right-click
      MainWIndow (Type)
      and select
      New
      Base controls
      Text box
      .
    2. Hover-over a gauge, select
      Edit
      , and enter:
      ValueTextBox
      .
    3. In the
      Properties
      pane, create a dynamic link between the
      Text
      property and
      ProjectName
      Model
      ConstrainedVariable
      For more information about dynamic links, see Create dynamic links.
Fornire un feedback
Hai domande o feedback su questa documentazione? invia il tuo feedback qui.
Normal