Create elements for controlling the max value
Create a label and a gauge to control the maximum value.
- Create the maximum value label:
- In theProject viewpane, right-clickMainWIndow (Type)and select .
- Hover-over the label, select, and enterMaxValueLabel.
- In thePropertiespane and set theTextproperty value toMaximum Value.
- Configure the max gauge:
- In theProject viewpane, right-clickMainWIndow (Type)and select .
- Hover-over the gauge, select, and enterMaxGauge.
- In thePropertiespane, create a dynamic link between theValueand .For more information about dynamic links, see Create dynamic links.
Fornire un feedback